Skip to main content

FAQ Search Results No. 1000484

FAQ 1000484

Latest Updated:2011年6月 24日

Functions: Build and Makefile ; Warnings & Errors ;

When the C/C++ compiler package for the RX family is upgraded to V.1.01 Release 00 and the attached sample program with the Renesas Starter Kit is built, an build error occurs.

Please rebuild after setting as follow:

  1. Launch RX Standard Toolchain from the Build Menu.
  2. In the 'C/C++:' entry box, add the entry:
    -secion=L=C

  3. Press 'OK' to close the RX Standard Toolchain dialog box.
  4. Rebuild the project.

Was this information useful to you? Yes NO

Suitable Products
Renesas Starter Kit+ for RX62N
Renesas Starter Kit for RX610
Renesas Starter Kit for RX62T

Related FAQs

No Related FAQs


End of content

Back To Top