FAQ Search Results No. 1000358
FAQ 1000358
Latest Updated:2011年3月 31日
Functions: Operating Environment ;
Can the CPU board operate on 3.3 V supplied from an emulator or an AC adapter?
Although supplying 3.3 V from an emulator or an AC adapter will not cause problems for operation, at 3.3 V operation the attached LCD module will not be able to display.
Also, when connecting the CPU board to an external board, make sure to separate the 5 V and 3.3 V power supply systems. For details, please refer to the circuit diagram and the section in the user's manual about option links.
Was this information useful to you? Yes NO
Suitable Products| Renesas Starter Kit for SH7086 |
| Renesas Starter Kit for M16C/26A |
| Renesas Starter Kit for R8C/13 |
| Renesas Starter Kit for R8C/1B |
| Renesas Starter Kit for M16C/6NK |
| Renesas Starter Kit for R8C/35C |
| Renesas Starter Kit for R8C/L3AC |
| Renesas Starter Kit for R8C/LA8A |
| Renesas Starter Kit for M16C/29 |
| Renesas Starter Kit for M16C/62P |
| Renesas Starter Kit for M32C/87 |
| Renesas Starter Kit for R32C/111 |
| Renesas Starter Kit for R32C/118 |
| Renesas Starter Kit for R8C/23 |
| Renesas Starter Kit for R8C/25 |
| Renesas Starter Kit for R8C/27 |
| Renesas Starter Kit for R8C/2D |
| Renesas Starter Kit for H8/38347 |
| Renesas Starter Kit for 3803L |
| Renesas Starter Kit for 38D5 |
| Renesas Starter Kit for 7542 |
Americas