FAQ Search Results No. 1000601
FAQ 1000601
Latest Updated:09/30/2011
Functions: Other Timer/Pulse Function ;
The TRCGRB register is used for the timer RC input capture function. Even if the CCLR bit in the TRCCR1 register is set to 1, the TRC counter is not cleared to 0000h by the input capture.
When setting the CCLR bit to 1, the TRC counter can only be cleared to 0000h by the TRCGRA input capture or TRCGRA compare match. The TRC counter CANNOT be cleared using registers TRCGRB, TRCGRC, and TRCGRD.
Was this information useful to you? Yes NO
Suitable Products| R8C/3x |
| R8C/Lx |
Americas