|
Promotional Part Number:R5F56216BDFP
The RX621 Group and the RX62N Group are built around the RX core and are equipped with 2 channels (max) of USB 2.0 full-speed (Host, Function and OTG), 2 channels of CAN*, and EtherMAC** as communications interfaces. The products are designed to not put a restriction on applications based on their communication method, and these communication methods can be achieved on a single chip. They are also equipped with a rich set of system fail-safe functions such as power-on reset (POR), low voltage detection (LVD), and an independent watchdog timer. *Optional setting for RX62N Group. **Only available for RX62N Group.
|