RI600/PX Real-time OS for RX Family
Target device
RX600 series with MPU (Memory Protection Unit)
Overview
The RI600/PX was developed based on the RI600/4, which conforms to the latest version of μITRON 4.0 specification and with additional memory protection function of the μITRON 4.0 protection extension. Almost all service calls in it except Rendezvous are supported.
- * Only the memory object protect function of µITRON 4.0 Specification for Protect Function Extension is supported, and the kernel object protect function is not supported.
- * T-Engine Forum holds the copyright on the μITRON Specification.
- * TRON, ITRON, and μITRON do not refer to any specific product or products.
Americas