Skip to main content

Flash Memory Reprogramming Kit by UART (M3A-2145G50) for M32R/ECU series

This product has been decided to discontinue selling.

The M3A-2145G50 connects the host PC's serial port to the M32R/ECU MCU serial I/O port on the evaluation board for starter kits and is a kit which realizes reprogramming control to the on-chip flash memory via direct UART communication with the flash reprogramming firmware which is stored in the M32R/ECU on-chip boot ROM. The M3S-UFLA32R is an on-chip flash memory reprogramming utility via UART communication and is built-in to the M3A-2145G50.

Combination with target MCU and target board

Target MCU Starter kit
32170/32174 group MCU M3A-2114G52, M3A-2114G52A
32171 group MCU M3A-2114G62, M3A-2114G62A
32172/32173 group MCU M3A-2114G72, M3A-2114G72A
32176 group MCU M3A-2152G52, M3A-2152G52A
32180 group MCU M3A-2142G52, M3A-2142G52A
32182 group MCU M3A-2142G62, M3A-2142G62A
32185/32186 group MCU M3A-2154G52B
32192/32195/32196 group MCU M3A-2154G52B, M3A-2154G52A

The object for M3S-UFLA32R can be downloaded from following.
M3S-UFLA32R executable file (ZIP:3.59MB)


End of content

Back To Top