Skip to main content

Collaboration with MATLAB

MATLAB is a technical computing software application developed by The MathWorks Inc. It can be used in engineering and many other fields.

  • Interaction with RTW-EC
    Modeling by MATLAB, and code generated by Real Time Workshop-Embedded Coder (RTW-EC), are automatically exported to High-performance Embedded Workshop (HEW).
  • Co-simulation is supported between MATLAB/Simulink and HEW.

* MATLAB is a modeling tool by The MathWorks Inc. (U.S.).
* Simulink is a model verification tool by The MathWorks Inc. (U.S.).
* The Real-Time Workshop Embedded Coder (RTW-EC) is a C source code generation tool by The MathWorks Inc. (U.S.).
* This tool is supported by Renesas and The MathWorks, Inc.
* Please contact a Renesas sales office to request the tool.



Collaboration with Cantata++

Cantata++ is a unit/integration test support tool that makes unit tests more efficient and reduces the number of man hours for testing software.

  • A Cantata++ wizard (TestDriver) can be started and programs tested directly from Renesas' High-performance Embedded Workshop (HEW) integrated development environment.
  • A high-precision test can be performed using the same CPU instruction set as the system.
  • This tool can be customized for application to various CPUs or compiler versions.



End of content

Back To Top