Overview
Integrated development environment CubeSuite (Cube suite) offers the ultimate in simplicity, usability, and security for the repetitive editing, building and debugging that typifies software development. Easy to install and operate, CubeSuite offers a highly user-friendly development environment featuring significantly shorter build times and graphical debug functions. The robust lineup of expanded functions and user support functions ensures a dependable environment for all users.
The CubeSuite was shifted to the new product CubeSuite+. When you would like to use it, please consider CubeSuite+.
Features

- Easier to use
- The platform is easy for anyone to use. An intuitive GUI makes procedures common across tools. Tutorials are also provided, so even beginners do not need advanced instruction or training.
-
- Tutorials are available for everything from creating programs to debugging and writing programs to the microcontroller. Anyone can get started using CubeSuite easily, by following the step-by-step instructions in the tutorials.
-
-
- CubeSuite supports the unique development styles of your developers. The program windows can be freely customized using docking, floating, auto-hide, and other features. You can also configure the menus and icons to your preferences.
-
-
- All settings can be managed from the Properties panel. The display changes each time a node is selected from the Project Tree, making it easy to find and configure the settings.
-
-
- The project tree is categorized according to the microcontroller development flow. This powerful tool enables you to switch to the desired task simply by clicking on a node.
-
-
- Configure the processing of dual-use pins in the pin list, while checking pin layout in the Top View. Paste the top view into the design documents, or save the pin list as an Excel file.
-
-
- Automatically generate programs (device/driver programs) to control the microcontroller's peripheral functions (e.g. timer, UART, and A/D) via graphical user interface (GUI) settings.
Note: Some devices may not be supported. -
-
- Builds in conventional development environments took a lot of time: you would have to edit all the source files, and then execute a build again. CubeSuite greatly reduces build times with a "rapid build" feature that automatically executes builds in the background when a source file is modified or saved.
-

- Full maintenance and support features
- CubeSuite is always there to support you. We offer powerful support both during and after development, including tool updates, technical support, and backups.
-
- With CubeSuite’s update features, you can check and download the latest version of their tools easily. With this features, you can ensure that your environment is always up to date.
-
-
- Get the technical support if you’re having any problems. You can easily extract the information about your tool which is necessary for seeking technical support (Eg: version information). You can copy all the information from the support form and send the inquiry to support representative.
-
-
- CubeSuite offers powerful backup features, enabling you to back up and restore your projects and tools with a single operation. This is great for users who want to develop derivative programs, or who want to back up their environment in case a bug appears after a product is complete.
-
CubeSuite and Development Environment
Use CubeSuite together with IECUBE, MINICUBE, MINICUBE2, and other software tools for a powerful and user-friendly development environment.
Cube Suite Combination of Tools and Hardware

Target Devices
For details, refer to the list below.
| Title | Date updated
| Size | Download |
CubeSuite Target devices and support functions list |
Dec 26. 2011 |
140KB |
 |