Device File Updater
- Overview
- Downloads
- Design Support
- Further Information
Overview
To respond to the rapid development of Renesas devices (CPU), Renesas provides the "Device File Updater" for the Renesas IDE, High-performance Embedded Workshop.
The Device File Updater is the program that adds new devices (CPU) to the target CPU type select list* of the High-performance Embedded Workshop.
* The CPU type select list appears when you create a new project workspace (see below figure).

Types of Device File Updater
The Device File Updater is released depending on the compiler package for High-performance Embedded Workshop :
- Device File Updater for C/C++ Compiler Package for SuperH Family
- Device File Updater for C/C++ Compiler Package for RX Family
- Device File Updater for C Compiler Package for R32C Series
- Device File Updater for C Compiler Package for M16C Series and R8C Family [M3T-NC30WA]
- Device File Updater for C/C++ Compiler Package for H8SX, H8S, H8 Family
Support Information
- The latest programs can be downloaded from the Download site.
- For details about the release information, see ToolNews.
- For details about the added CPUs, please refer to the PDF file below.
Americas