Auto Update Utility
- Overview
- Downloads
- Design Support
- Further Information
- Basic Procedure
- How to Use
- How to Startup
- Tools Supported
- Operating Environment
Basic Procedure
![]() | ![]() |
| ・Install Auto Update Utility (When installing Renesas tools, you can also install Auto Update Utility at the same time.) | |
| ↓ | |
| ・Register the tools for Auto Update Utility (This setting registers automatically when you perform an initial installation and an update program of the tool.) | |
| ↓ | |
| ・Complete the initial settings (Auto Update Utility icon is displayed in the task bar.) |
| ↓ |
![]() | ![]() |
1. Auto Update Utility checks for update information For details, see "How to Use".(Auto checking via the Internet. By default, auto-launch once a week.) | |
| ↓ | |
| 2. Auto Update Utility informs user (If update information is found, a message is shown in the task bar.) | |
| ↓ | |
| 3. Execute the update program (By selecting tools to be updated from the list, the update program(s) will be executed.) |
[To confirm the registered Renesas tools]
Click the Auto Update Utility icon in the task bar. ↓ You can confirm the registered Renesas tools on the list in Auto Update Utility.
|
Americas





For details, see "