HS0008EAUF1H (Discontinued product)
Marketing of the HS0008EAUF1H has been discontinued. The successor to HS0008EAUF1H is E8a.

Target Devices
HS0008EAUF1H accepts all devices including Vcc/ PVcc mixed spec-compliant devices, but not 12V-applied programming spec-compliant devices.
Devices being not supported in FDT are checked off also.
For the latest information about target MCUs and programming software, refer to the following PDF. (The colored cells were updated by the latest version.)
| File name | Download |
| Flash programming tools target device list | |
Information about the target MCUs when using HS0008EAUF1H with Flash Development Toolkit Ver.3 (previous version) is here.
Overview
The flash microcomputer on-board programming adapter board HS0008EAUF1H, connected between a host computer and the user system, can program/erase user application programs on the flash memory incorporated in the flash microcomputer on the user system (on-board) when it is used with Flash Development Toolkit (hereinafter referred to as FDT). Therefore, the burden on peripheral circuit required during on-board programming can be reduced.
An input power is supplied via USB interface. (Performs by a bus power of host PC)
PC Interface
USB interface (Compliant with USB Specification Rev1.1)
Product components
| No. | Packaged Items | Description | Quantity |
| 1 | Adapter board | Main unit | 1 |
| 2 | User system interface cable (290mm)* | Connection between main unit and user system | 1 |
| 3 | User system interface cable connector | Connection between main unit and user system | 1 |
| 4 | USB cable (2000mm) | Connection between main unit and host computer | 1 |
| 5 | Flash Development Toolkit setup program and user's manual (provided on a CD-R) | R0C00000FDW04R | 1 license |
| 6 | Adapter board user's manual | HS0008EAUF1HE | 1 |
| 7 | Description Notes on Handling Control Pins with the Adapter Board Connected | HS0008EAUF1HE-N | 1 |
*At shipment, the user systemcable is connected the main unit.
Americas