Skip to main content

Introduction

The E10T is a low-cost emulator from Renesas released . The E10T is designed to be used in conjunction with the on-chip debugging interface, currently implemented on members of the H8/300H and the new H8/300H Tiny series of microcontrollers.

The E10T provides real time debugging on the target device, using dedicated debugging resources on the target micro-controller in the users hardware. The E10T interfaces to the users target system via an interface which can be used both to debug the system and to program the microcontroller's on-chip Flash memory.

The E10T comes in two versions, a PCMCIA version, ideal for laptop computers, and a PCI version for desktop machines.

Features

  • 255 PC Breakpoints
  • 1 Hardware breakpoint on data and address
  • 4 level PC branch trace
  • On-chip Flash programming
  • C source level debugger
  • Support for Windows® 2000, XP

Related Resources


End of content

Back To Top