HS0005KCU02H
![]() HS0005KCU02H* (Supporting AUD trace function) | >> Click here to the front page of E10A-USB. | |||
![]() HS0005KCU01H* (Not supporting AUD trace function) | ![]() HS0005KCU14H (For SuperH RISC engine Family of multi-core MCUs) | |||
* When using with an MCU of SH7147 or SH7142 Group, Debug MCU Board (HS7147EDB01H) is required. |
Overview
HS0005KCU02H is an on-chip debugging emulator which utilizes H-UDI interface
of the target device and supports AUD - Advance User Debugging where this
capability is supported by the target device.
The AUD is supported via 36-pin cable, the H-UDI can be connected using the
14-way cable.
Components
- E10A USB supporting H-UDI and AUD trace - HS0005KCU02H
- 14-way cable for H-UDI connection
- 36-way cable for AUD support
- Installation CD incorporating
- High-performance Embedded Workshop integrated development environment with the E10A-USB debugger component
- All device addition options
PC interface
USB interface (USB 1.1, Full speed)
Notes:
No C/C++ compiler toolchains are included. When initially programming the E10A-USB the user will assign a device group personality to the E10A-USB. This is a one time process (OTP) and cannot be changed. Please refer to the E10A-USB Product Configration for further details.
Americas