Skip to main content


HS0005KCU01H*
(Not supporting AUD trace function)
>> Click here to the front page of E10A-USB.

HS0005KCU02H*
(Supporting AUD trace function)


HS0005KCU14H
(For SuperH RISC engine Family
of multi-core MCUs)

* When using with an MCU of SH7147 or SH7142 Group, Debug MCU Board (HS7147EDB01H) is required.

 

Overview

HS0005KCU01H is an on-chip debugging emulator which utilizes H-UDI interface of the target device.
The H-UDI can be connected using the 14-pin cable.
HS0005KCU01H does not support AUD trace functionality and is available at a lower price than the HS0005KCU02H which supports AUD.

Components

  • E10A USB supporting H-UDI only - HS0005KCU01H
  • 14-way cable for H-UDI connection
  • Installation CD incorporating
    • High-performance Embedded Workshop integrated development environment with the E10A-USB debugger component
    • All device addition options

PC interface

USB interface (USB 1.1, Full speed)

Notes:

No C/C++ compiler toolchains are included. When initially programming the E10A-USB the user will assign a device group personality to the E10A-USB. This is a one time process (OTP) and cannot be changed. Please refer to the E10A-USB Product Configuration for further details.


End of content

Back To Top