Skip to main content

E10A-USB LITE

Introduction

E10A-USB LITE - Automatic support for all H8S, H8SX and SH2 microcontrollers with H-UDI interface. (Does not support SH2, SH3 or SH4 microprocessors.)

HS0005KCU11H is an on-chip debugging module which utilizes the H-UDI interface of the target device. The H-UDI can be connected using the 14-pin cable. This module does not support the AUD interface, for AUD support please use the HS0005KC02H E10A-USB.

Components

  • E10A USB supporting H-UDI only - HS0005KCU11H
  • 14-way cable for H-UDI connection
  • Installation CD incorporating
    • High-performance Embedded Workshop integrated development environment with the E10A-USB debugger component
    • Support for H8S, H8SX and SH2 microcontrollers with H-UDI interface. No support for SH3 or SH4 and no need to install Device Group Additions.

 

PC Interface

USB interface (USB 1.1, Full speed)


End of content

Back To Top