R8C UART Monitor Program
R8C UART Monitor Program
Information(11 May 2011)
The update program supporting R8C/1x, R8C/2x, R8C/3x、R8C/Lx and R8C/Mx has been updated. (High-performance Embedded Workshop version only)
You can download the program from "Downloads" in the left navigation on this page.
- For R8C/3xA, M Groups, use “R8C/3xC Group”
- For R8C/LxA, B Groups, use “R8C/LxC Group”
- After the Monitor Program is written to the MCU and the Monitor Program communicates with the Debugger, the user program can be debugged. Use RS-232C for communication between the Debugger and the Monitor Program.
- The Monitor Program is automatically written to the MCU when the Debugger is started up. Therefore, there is no need to write the Monitor Program to the MCU using a flash programmer.
- You can debug by the same pin handling as Standard Serial I/O Mode 2 for the flash programmer.
- Initialize (erase) the user program area using a flash programmer before using the Monitor Program.
Target Devices
M16C R8C FoUSB/UART debugger (High-performance Embedded Workshop Version)
The debugger depends on your MCU. In addition, the High-performance Embedded Workshop version of the debugger is the successor debugger of the KD30/KD3083 version. The High-performance Embedded Workshop version is only scheduled for release in the future.
| Family | Series | Group | Part No. | ||
|---|---|---|---|---|---|
| R8C | R8C/1x | R8C/10 | R5F21102 | R5F21103 | R5F21104 |
| R8C/11 | R5F21112 | R5F21113 | R5F21114 | ||
| R8C/12 | R5F21122 | R5F21123 | R5F21124 | ||
| R8C/13 | R5F21132 | R5F21133 | R5F21134 | ||
| R8C/14 | R5F21142 | R5F21143 | R5F21144 | ||
| R8C/15 | R5F21152 | R5F21153 | R5F21154 | ||
| R8C/16 | R5F21162 | R5F21163 | R5F21164 | ||
| R8C/17 | R5F21172 | R5F21173 | R5F21174 | ||
| R8C/18 | R5F21181 | R5F21182 | R5F21183 | ||
| R5F21184 | - | - | |||
| R8C/19 | R5F21191 | R5F21192 | R5F21193 | ||
| R5F21194 | - | - | |||
| R8C/1A | R5F211A1 | R5F211A2 | R5F211A3 | ||
| R5F211A4 | - | - | |||
| R8C/1B | R5F211B1 |
R5F211B2 | R5F211B3 | ||
| R5F211B4 | - | - | |||
| R8C/2x | R8C/20 | R5F21206 | R5F21207 | R5F21208 | |
| R8C/21 | R5F21216 | R5F21217 | R5F21218 | ||
| R8C/22 | R5F21226 | R5F21227 | R5F21228 | ||
| R8C/23 | R5F21236 | R5F21237 | R5F21238 | ||
| R8C/24 | R5F21244 | R5F21246 | R5F21247 | ||
| R5F21248 | - | - | |||
| R8C/25 | R5F21254 | R5F21256 | R5F21257 | ||
| R5F21258 | - | - | |||
| R8C/26 | R5F21262 | R5F21264 | R5F21265 | ||
| R5F21266 | - | - | |||
| R8C/27 | R5F21272 | R5F21274 | R5F21275 | ||
| R5F21276 | - | - | |||
| R8C/28 | R5F21282 | R5F21284 | R5F21286 | ||
| R8C/29 | R5F21292 | R5F21294 | R5F21296 | ||
| R8C/2A | R5F212A7 | R5F212A8 | R5F212AA | ||
| R5F212AC | - | - | |||
| R8C/2B | R5F212B7 | R5F212B8 | R5F212BA | ||
| R5F212BC | - | - | |||
| R8C/2C | R5F212C7 | R5F212C8 | R5F212CA | ||
| R5F212CC | - | - | |||
| R8C/2D | R5F212D7 | R5F212D8 | R5F212DA | ||
| R5F212DC | - | - | |||
| R8C/2E | R5F212E2 | R5F212E4 | - | ||
| R8C/2F | R5F212F2 | R5F212F4 | - | ||
| R8C/2G | R5F212G4 | R5F212G5 | R5F212G6 | ||
| R8C/2H | R5F212H1 | R5F212H2 | - | ||
| R8C/2J | R5F212J0 | R5F212J1 | - | ||
| R8C/2K | R5F212K2 | R5F212K4 | - | ||
| R8C/2L | R5F212L2 | R5F212L4 | - | ||
| R8C/3x | R8C/32C | R5F21321C | R5F21322C | R5F21324C | |
| R8C/33C | R5F21331C | R5F21332C | R5F21334C | ||
| R5F21335C | R5F21336C | - | |||
| R8C/34C | R5F21344C | R5F21345C | R5F21346C | ||
| R8C/35C | R5F21354C | R5F21355C | R5F21356C | ||
| R5F21357C | R5F21358C | R5F2135AC | |||
| R5F2135CC | - | - | |||
| R8C/36C | R5F21364C | R5F21365C | R5F21366C | ||
| R5F21367C | R5F21368C | R5F2136AC | |||
| R5F2136CC | - | - | |||
| R8C/38C | R5F21386C | R5F21387C | R5F21388C | ||
| R5F2138AC | R5F2138CC | - | |||
| R8C/32D | R5F21321D | R5F21322D | R5F21324D | ||
| R8C/33D | R5F21331D | R5F21332D | R5F21334D | ||
| R5F21335D | R5F21336D | - | |||
| R8C/35D | R5F21354D | R5F21355D | R5F21356D | ||
| R8C/33T | R5F21334T | R5F21335T | R5F21336T | ||
| R8C/32M | R5F21321M | R5F21322M | R5F21324M | ||
| R8C/33M | R5F21331M | R5F21332M | R5F21334M | ||
| R5F21335M | R5F21336M | - | |||
| R8C/34M | R5F21344M | R5F21345M | R5F21346M | ||
| R8C/35M | R5F21354M | R5F21355M | R5F21356M | ||
| R5F21357M | R5F21358M | R5F2135AM | |||
| R5F2135CM | - | - | |||
| R8C/Lx | R8C/L35C | R5F2L357C | R5F2L358C | R5F2L35AC | |
| R5F2L35CC | - | - | |||
| R8C/L36C | R5F2L367C | R5F2L368C | R5F2L36AC | ||
| R5F2L36CC | - | - | |||
| R8C/L38C | R5F2L387C | R5F2L388C | R5F2L38AC | ||
| R5F2L38CC | - | - | |||
| R8C/L3AC | R5F2L3A7C | R5F2L3A8C | R5F2L3AAC | ||
| R5F2L3ACC | - | - | |||
| R8C/Mx | R8C/M11A | R5F2M111A | R5F2M112A | - | |
| R8C/M12A | R5F2M121A | R5F2M122A | - | ||
M16C R8C FoUSB/UART debugger (KD30 Version)
| Family | Series | Group | Part No. | ||
|---|---|---|---|---|---|
| R8C | R8C/1x | R8C/10 | R5F21102 | R5F21103 | R5F21104 |
| R8C/11 | R5F21112 | R5F21113 | R5F21114 | ||
| R8C/12 | R5F21122 | R5F21123 | R5F21124 | ||
| R8C/13 | R5F21132 | R5F21133 | R5F21134 | ||
| R8C/14 | R5F21142 | R5F21143 | R5F21144 | ||
| R8C/15 | R5F21152 | R5F21153 | R5F21154 | ||
| R8C/16 | R5F21162 | R5F21163 | R5F21164 | ||
| R8C/17 | R5F21172 | R5F21173 | R5F21174 | ||
System Configuration

Preparations
- PC with Serial Port
- Communication Cable
- Target Board, Power Supply
- Debugger
* You can download the Debugger from "Downloads" button in the left menu.
Operating Environment
The operating environment depends on your debugger.
M16C R8C FoUSB/UART debugger (High-performance Embedded Workshop Version)
| PC | IBM PC/AT or compatible PC with Intel Pentium III 600MHz or higher |
|---|---|
| OS | Windows XP, Windows 2000, Windows ME, Windows 98 SE (98) |
| Memory | 128MB or higher |
| Interface | 9-pin D-SUB Serial Interface |
M16C R8C FoUSB/UART debugger (KD30 Version)
| PC | IBM PC/AT or compatible PC with Intel DX4 100MHz/Pentium II 75MHz or higher |
|---|---|
| OS | Windows XP, Windows 2000, Windows ME, Windows 98 SE (98), Windows 95 |
| Memory | 16MB or higher |
| Interface | 9-pin D-SUB Serial Interface |
Americas