|
Introduction - IO Wizard aids new Renesas microcomputer (MCU) users to make initialization setting in the source code.
- IO Wizard serves as a jumpstart for software engineers or students starting Renesas MCU based projects helping them speed up their software development process.
|
 |
Features |
 |
- User input the device selection, system setting and peripheral operation setting through GUI.
- A status window is provided allowing user to see the actual source code generated in real time according to the selection on the GUI .
- After all setting are done, user can proceed to run code generation.
- The output files have to go through code compilation process before user can obtain the object file.
- Support of interrupt settings for peripheral functions (R8C devices only).
- Link to HEW feature is added. This feature allows user to insert the generated source codes into HEW.
- Save and Load feature is added. This feature allows user to load and save settings.
- Compatible with Windows Vista (R).
|
 |
Technical Support |
 |
IO Wizard is a free of charge and "AS IS" basis software. No support will be provided for this software. It is the responsibility of the user to verify the code generated is suitable for their application. The user assumes the entire risk of using the products. |
 |