Application Builders
"Faster time to market" is a goal that all project leaders are seeking. As the complexity of the on chip peripherals increase there is equally increasing pressure on that time taken to generate the necessary low level drivers. Traditionally these drivers have been written by engineers, after much thumbing through hefty data books.
Now Renesas in co-operation with our industry partners offer a range of time-saving software packages to aid developers in creating these necessary low-level drivers.
Americas