Board ID Use Cases
- Overview
- Contact Us
- Alliance Partners
- Further Information
- 1. Secure Tracking
- 2. Anti-cloning
- 3. Usage Control
- 4. IP Protection
Anti-cloning

This use case describes an application in which the host device is required to enforce authentication; that is, refuse to accept an unauthorized peripheral. The design challenge here is to find a robust way to implement security across the entire system, because weak points in the design might allow circumvention of the enforcement mechanism.
This application differs from the Board ID™ tracking use case in which a person performs the enforcement function. Also, it differs from a simple authentication scenario in which the device does not need to have a unique identity, but only has to prove to the host that it is authentic.
The Board ID Demonstration Kit includes a demo that shows how the Board ID chip can ensure that the host device can use only an authenticated peripheral.
For more information on Board ID, visit the FAQ page
Americas