Skip to main content

  • Application Examples

Configuration example of Web cameras using the SuperH family

- Realize high-quality real-time image -> Ethernet effectiveness: 2.4Mbps, 320x240(30fps)
- A built-in system platform in the main body of the camera via the adoption of CSP (14mm2).


Configuration example of DVD recorders using the SuperH family

DVD recorders can be connected easily by connecting the SH7618 to DVD main system.
Realize program listing download by EPG and remote record system by a mobile-phone.

* EPG: Electronic Program Guide



End of content

Back To Top