Application examples - Cleaner
Configuration example of cleaners using the SuperH family
This is an example of motor control of cleaners using the SH7046. The SH7046 is equipped with the high performance 32-bit RISC core, two multifunctional timers for motor control and multi channel A/D converter. The SH7046 can realize inverter control and sensor inputs by one chip.

Americas