Skip to main content

Application examples - Air conditioner outdoor unit

Configuration example of air conditioner outdoor units using the SuperH family

This is an example of air conditioner outdoor units using the SH7146. The SH7146 is equipped with high performance 32-bit RISC core, two multifunctional timers for motor control and multi-channel A/D converter. The SH7146 can realize inverter and converter control by one chip.



End of content

Back To Top