RX Family
What's New
05 Apr 2012
To see all issues of the RX News, See the RX News page.


The RX family offers mid-range MCUs that Renesas proudly proclaims will be the next-generation world standard of the #1 MCU supplier.

RX is a revolutionary new core developed by the world's #1 microcontroller supplier, Renesas Electronics. Follow the link here to learn more about this advanced 32-bit core that includes floating point operations and built in digital signal processing capabilities.
Read more about The Core Difference
RX 32-bit MCU Family - The Core Difference in Your Design
These next generation microcontrollers based on the revolutionary RX CPU core enable a new class of MCUs blending the best traits of RISC and CISC MCU architectures while adding DSP and floating point math capability.
This hybrid Digital Signal Controller approach meets the demands of today's embedded applications requiring high performance yet very low power consumption; the smallest possible code and data size; the lowest cost; and the need for digital signal processing.
Drawing from a rich heritage of existing CPU cores from the world's #1 MCU supplier, the RX CPU core design leads the industry for performance and capability in embedded MCUs. There are two compatible RX series to best match your needs starting with RX600 for extreme performance and connectivity, followed by RX200 for ultra-low power applications. Tools, firmware libraries, and documentation make it easy to migrate to RX from any other MCU platform, or to start a new RX design.
RX600
RX610 General Purpose
These groups come with a rich set of communication peripherals such as Ethernet MAC, USB 2.0 full-speed (Host, Device, and OTG), and CAN. They are also equipped with several DMA controllers including a dedicated External DMA controller which can be used to drive a TFT-LCD.
>View Products
RX621, RX62N Connectivity
These groups come with a rich set of communication peripherals such as Ethernet MAC, USB 2.0 full-speed (Host, Device, and OTG), and CAN. They are also equipped with several DMA controllers including a dedicated External DMA controller which can be used to drive a TFT-LCD.
>View Products
RX62T Motor & Inverter Control
Optimized for motor control and inverter control applications, the RX62T devices include advanced PWM timers and advanced analog-to-digital converter sub-systems with six programmable op amps, six sample/hold circuits, and six window comparators. With one RX62T device, it is possible to drive two three phase motors at the same time.
>View Products
RX630 Group

The RX630 Group has only 2.5uA standby power and enhanced analog, communication, and timer functions. The products are equipped with 21 channels of 12-bit A/D and another 8 channels of 10-bit A/D making up to 29 A/D channels available.
>View Products
RX631 Group

Offering only 2.5uA standby power; the RX631 Group is built around the RX core and is equipped with 2 channels of USB 2.0 full-speed (Host, Function and OTG) and up to 3 CAN channels.
>View Products
RX63N Group

The RX63N Group is built around the RX core and comes equipped with an Ethernet 10/100 MAC with DMA. The RX63N Group also includes 2 channels of USB 2.0 Full-Speed (Host, Function and OTG), 3 channels of CAN interface, 4 I2C, 13 SCI, 3 SPI, and an external bus.
>View Products
RX63T Group

The RX63T Group is a complement to the RX62T group, bringing lower memory, lower pin-count variants and featuring enhanced safety functions over the RX62T Group. In addition to its use as a general-purpose microcontroller (MCU), the RX63T is a cost effective solution for single vector motor control in consumer devices and industrial equipments.
>View Products
RX200
RX210 General Purpose
RX210 Flash MCUs bring new levels of capability and performance to ultra-low-power, low-voltage embedded-system applications. Based on the fast 32-bit RX CPU core, RX210 chips are the first members of the RX200 series of middle-range products.
>View Products
Lineup:
RX200
The low power series of the RX Family. The RX200 product series combines the high calculation performance of the RX600 and new low power and safety capabilities.
RX600
The RX600 is the high-speed and high-performance series in the RX family.
The series is positioned as the upward successor to the H8SX and R32C, the 32-bit families of Renesas MCUs.
RX610 | RX621, RX62N | RX62G | RX62T | RX630 | RX63N, 631 | RX63T
Americas