Skip to main content

Compatibility with existing Renesas products
Using the MCU Development Platform to facilitate new RX MCUs

The RX family represents a huge upgrade in functionality from existing Renesas MCUs, yet it achieves compatibility with existing devices in our H8S, H8SX, M16C, and R32C families. For example, for endian data access, the RX CPU architecture allows a choice between the big- and little-endian formats. The new RX MCUs support endian format conversion instructions so system designs can inherit data formats, aiding the reuse of existing code.

To ease the transfer of peripheral functions from existing MCUs, Renesas has used a platform technology that was refined in the implementation of the EXREAL Platform, applying it to create a powerful and flexible new chip development support product: the MCU Development Platform (see Figure 3-1, below). It treats those functions as IP and turns them into assets. The platform's operational approach also facilitates the development of on-chip functions and eases the process of adding functions to chip designs. The greater design efficiency enabled by the capabilities of the MCU Development Platform shortens the time required to develop new RX MCUs. Also, by eliminating key differences between individual products, the platform facilitates feature migrations between product groups.

Fig. 3-1. Inheritance of Peripheral Functions by Use of MCU Development Platform

TAT reduction: Since peripheral functions can be developed in advance, the development
of new functions becomes easier
Faster rollout:Greater efficiency in design leads to smoother productrelease
Better usability: Less difference among products means smoother migration

Inheritance of Peripheral Functions by Use of MCU Development Platform

Table of Contents

Development of the RX family

The high-performance RX CPU architecture

Compatibility with existing Renesas products

RX family product lineup

System development environment for RX MCUs


End of content

Back To Top