Design kits
Synthesizable Core Design Kit (SCDK)
When to use a synthesizable core
Synthesizable core versions of our CPU products are designed for the following uses:
- Licensees who want to configure a CPU core for their application, for example changing the cache size.
- Licensees who want to layout the CPU with a specific aspect ratio that fits best with their other IP in the SoC.
- Porting to new silicon processes, for example targeting a low power variant or custom process such as SOI.
- Licensees with specific speed or power consumption targets not available in a standard hard core delivery.
Porting a synthesizable core
Porting a synthesizable core in to a new process can be performed by the licensee or one of the SuperH Partners, for example a Design Partner such as DNP or a Design Agency who have been trained and have experience in SuperH products.
The SCDK
The SCDK includes the scripts, RTL, test and validation suites that are required by a silicon design team to deliver a CPU port, including:
- Logical implementation environment
- Module Naming convention
- HDL Coding guidelines
- Front end implementation documents
- Constraints, synthesis & TA scripts etc.
- Full RTL simulation/synthesis environment
- Simulation/synthesis libraries which are required to compile, simulate and understand the design.
- Synthesisable and behavioral views as appropriate for full custom blocks.
- Compile scripts to enable a build of database
- Full custom implementation environment
- Macro implementation documents
- Verification environment – test vectors, expected results.
- Formal verification scripts,
- Characterization methodologies
- Physical implementation environment
- Back end implementation documents
- Clock Tree definition
- Floorplan Information
Americas