High-Precision Super Junction Structure Realizes Low Power Consumption for LCD TVs and PC Servers

January 12, 2011

TOKYO, January 12, 2011 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced the availability of a new high-voltage N-channel power metal-oxide-semiconductor field-effect-transistor (MOSFET) product, the RJK60S5DPK, for power supply units that delivers high efficiency. The new power MOSFET provides low power consumption for PC servers, communication base stations, and solar power generation systems.

The new RJK60S5DPK power MOSFET is ideal for use in the primary power switching circuit of a power supply unit, which converts alternating current (AC) to direct current (DC). It is the first product in Renesas Electronics' high-voltage power MOSFET series, which employs a high-precision super junction structure (Note 1) to achieve a figure of merit (FOM, Note 2), a key overall performance index for power MOSFET devices, that is approximately 90 percent improved from that of the company's existing products.

Recently, demand has grown for improved efficiency in the power supply circuits to reduce energy consumption, and there is a particularly strong demand for low power consumption though improved power conversion efficiency in high-output switching power supplies for flat-panel TVs, communication base stations, PC servers, and solar power generation systems, and this has spurred demand for power MOSFET products with lower on-resistance (Note 3). However, there are limits to the improvements that can be achieved using a conventional planar structure. Renesas Electronics therefore made use of its accumulated expertise in power device technology to develop a high-precision super junction structure employing a deep-groove formation process. This has made it possible to produce MOSFET devices with a lower on-resistance per unit of area.

Main features of the new RJK60S5DPK power MOSFET

(1) Industry-leading low on-resistance

The new RJK60S5DPK power MOSFET achieves an on-resistance of 150 milliohm (mΩ, standard value at ID = 10 A, VGSS = 10 V), approximately 52 percent lower than that of existing Renesas Electronics power MOSFET products. This reduces the amount of loss that occurs during power conversion.

(2) High-speed switching

Renesas Electronics' new power MOSFET has a drive capacitance (gate charge Qgd, Note 4), which affects the switching speed, of only 6 nC (nanocoulomb, standard value at ID = 10 A, VGSS = 10 V), approximately 80 percent less than that of existing Renesas Electronics products. This makes it possible to boost power conversion efficiency through the use of high-speed switching.

The package of the new RJK60S5DPK power MOSFET is equivalent in size to the TO-3P standard package, and the pin assignments conform to the industry standard. This means it can easily be mounted on switching power supply circuit boards that have been evaluated using conventional planar MOSFET devices.

The products in the high-precision super junction structure power MOSFET series can deliver on-resistance per unit of area approximately 80 percent lower than that of products in the company's existing planar structure series, so if the on-resistance remains the same the chip area can be decreased. Taking advantage of this, Renesas Electronics plans to release in the future a variety of power device products with smaller package sizes, such as products using the TO-220FL (10 mm × 15 mm) package that provide the performance of existing products using the TO-3P (15.6 mm × 19.9 mm) package.

In addition, Renesas Electronics has identified flat-panel TVs, communication base stations, and PC servers as products that can benefit from switching power supplies with reduced energy consumption, and the company plans to market a series of new ultra-low on-resistance MOSFET products targeted at such applications. Renesas Electronics intends to expand the scale of its high-voltage power device business by utilizing its technology expertise of the new RJK60S5DPK power MOSFET and develop a range of new products tailored for specific applications.

(Note 1) Super junction structure:
A structural configuration of power MOSFETs. Unlike a conventional planar structure, it enables lowering of the on-resistance without reducing the voltage tolerance of the device. This means the on-resistance per unit of area can be reduced. (See Note 3 regarding on-resistance.)

(Note 2) Figure of merit, or FOM:
An index of power MOSFET performance expressed as a numerical value obtained by multiplying the on-resistance (Ron) by the gate-drain charge capacitance (Qgd).

(Note 3) On-resistance (Ron):
The resistance when the power MOSFET is operating. A lower value indicates less conduction loss.

(Note 4) Gate-drain charge capacitance (Qgd):
The electric charge needed to make the power MOSFET operate. A lower value indicates faster switching performance.

The main specifications of the new RJK60S5DPK can be found in the separate sheet.

Pricing and Availability

Samples of Renesas Electronics' new RJK60S5DPK power MOSFET are available now, with a suggested price of US$5. Mass production is scheduled to begin starting April 2011 with a combined volume of 500,000 units per month projected by October 2011. (Pricing and availability are subject to change without notice.)

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All product and service names that appear in this press release are trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on